AXIS#.MOTOR.IDDATAVALID
Description
AXIS#.MOTOR.IDDATAVALID reports the status of the motor memory status.
The valid values for this keyword are the following:
|
Value |
Description |
|---|---|
|
0 |
Error in identification |
|
1 |
Success in identification |
|
2 |
Identification in process |
|
3 |
Identification not started yet |
|
4 |
Success recognizing feedback, but failed to varify OEM data integrity |
Context
For more information see Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.MOTOR.IDDATAVALID |
500bh |
2dh |
Unsigned8 |
- |
- |
Read only |
No |
|
AXIS2.MOTOR.IDDATAVALID |
510bh |
2dh |
Unsigned8 |
- |
- |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
6205 |
1 |
6205 (0x183d) |
AXIS1.MOTOR.IDDATAVALID |
Unsigned8 |
Read Only |
Yes |
|
71741 |
2 |
6205 (0x183d) |
AXIS2.MOTOR.IDDATAVALID |
Unsigned8 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.MOTOR.IDDATAVALID |
6205 |
Unsigned8 |
Read Only |
- |